Cancel
Showing results for 
Search instead for 
Did you mean: 

Deleting a duplicate file in one DXF- See example

Creator
Creator

We received these files when we purchased our CNC- The software is indeed SE-2D. I have tried everythign to just DELETE the upper Jeep image as a whole- its incomplete and I really only need the bottom one which is the completed one- MANY of the files have this issue. PLEASE PLEASE if you could do a quick video that would be really helpful. 

7 REPLIES

Re: Deleting a duplicate file in one DXF- See example

Gears Phenom Gears Phenom
Gears Phenom

fence select and delete worked just fine for me???

 

did you try that?

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Deleting a duplicate file in one DXF- See example

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Deawn,

 

As @Johnson_BigMatt says......fence select > delete [key], works as expected.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Deleting a duplicate file in one DXF- See example

Creator
Creator

When I try to do this, it does not turn pink, nor bring up the additional box in the video. 

 

https://www.youtube.com/watch?v=uHBXdGqCsFs

 

AND I dont know how to post a direct video, so the above link goes to YouTube. 

Re: Deleting a duplicate file in one DXF- See example

Siemens Phenom Siemens Phenom
Siemens Phenom

In your Select toolbar, open the Select Options -- the notepad looking icon on the left-hand side beside the "Direction Fence" pulldown.

 

In the Select Options set it to "All layers" and select OK.

 

Now use your directional fence select.

Highlighted

Re: Deleting a duplicate file in one DXF- See example

Creator
Creator

I have tried that as well.  I also watched another person be able to do it with my file I uploaded. I am just lost on the program. I wish they had people that could train on this software or an online class. 

Re: Deleting a duplicate file in one DXF- See example

Siemens Phenom Siemens Phenom
Siemens Phenom

Instead of posting the DXF file perhaps you should post the Solid Edge file you created after importing the DXF file.

Re: Deleting a duplicate file in one DXF- See example

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are a number of Solid Edge Partners that offer training and there is also a wealth of self-paced training and tutorials in the Solid Edge Help system.  Another helpful resource might be YouTube.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com