Cancel
Showing results for 
Search instead for 
Did you mean: 

Deleting a duplicate file in one DXF- See example

Creator
Creator

We received these files when we purchased our CNC- The software is indeed SE-2D. I have tried everythign to just DELETE the upper Jeep image as a whole- its incomplete and I really only need the bottom one which is the completed one- MANY of the files have this issue. PLEASE PLEASE if you could do a quick video that would be really helpful. 

7 REPLIES 7

Re: Deleting a duplicate file in one DXF- See example

Gears Phenom Gears Phenom
Gears Phenom

fence select and delete worked just fine for me???

 

did you try that?

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Deleting a duplicate file in one DXF- See example

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Deawn,

 

As @Johnson_BigMatt says......fence select > delete [key], works as expected.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Deleting a duplicate file in one DXF- See example

Creator
Creator

When I try to do this, it does not turn pink, nor bring up the additional box in the video. 

 

https://www.youtube.com/watch?v=uHBXdGqCsFs

 

AND I dont know how to post a direct video, so the above link goes to YouTube. 

Re: Deleting a duplicate file in one DXF- See example

Siemens Phenom Siemens Phenom
Siemens Phenom

In your Select toolbar, open the Select Options -- the notepad looking icon on the left-hand side beside the "Direction Fence" pulldown.

 

In the Select Options set it to "All layers" and select OK.

 

Now use your directional fence select.

Re: Deleting a duplicate file in one DXF- See example

Creator
Creator

I have tried that as well.  I also watched another person be able to do it with my file I uploaded. I am just lost on the program. I wish they had people that could train on this software or an online class. 

Re: Deleting a duplicate file in one DXF- See example

Siemens Phenom Siemens Phenom
Siemens Phenom

Instead of posting the DXF file perhaps you should post the Solid Edge file you created after importing the DXF file.

Re: Deleting a duplicate file in one DXF- See example

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are a number of Solid Edge Partners that offer training and there is also a wealth of self-paced training and tutorials in the Solid Edge Help system.  Another helpful resource might be YouTube.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com