Cancel
Showing results for 
Search instead for 
Did you mean: 

Design Manager, Do you want to proceed with the same location annoying

Legend
Legend

When using the save as command and writing into the same directory an very annoying warning is flagged.

 

My intention is to write a copy of a drawing or model into the same directory.

 

New versus Current same.jpg

 

Is there a way to stop this warning from flagging up.

 

Kind Regards,

 

Jan Bos

The Netherlands

See you all soon at Solid Edge University 2016

4 REPLIES 4

Re: Design Manager, Do you want to proceed with the same location annoying

Phenom
Phenom

I would have thought you'd have to also change the filename.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Design Manager, Do you want to proceed with the same location annoying

Legend
Legend
I am changing the filename, but the path stays the same..

Re: Design Manager, Do you want to proceed with the same location annoying

Phenom
Phenom

OK, sorry - I should have zoomed in a bit more.

I'm still on ST7 so can't really help any further.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Design Manager, Do you want to proceed with the same location annoying

Honored Contributor
Honored Contributor

Sometimes you have to do a bubble sort method. Chaning the names then restarting the manager. Then using the manager for what you really want. Then changing the names back if desired.