Cancel
Showing results for 
Search instead for 
Did you mean: 

Design Manager Performance issue

Legend
Legend

Hello,

the performance of the new design manager when selecting/deselecting files is catastrophic!

I have an assembly with about 5000 parts (800 unique). in the first step i choose "select all" and then "save as". In the dialog i choose "keep structure" (i don't know the exact descriptions because i use the german version). This command is slow, but it's acceptable.

In the next step i "select all", and then "choose files" to deselect some files. This is when the big problem starts. I have three text patterns of files i would like to deselect befor searching for the related drawings:

  • *Kaufteile*
  • *Standard Parts*
  • *Frames*

Deselecting of one Pattern takes about 30-45 minutes! At the beginning of the process, i can watch how slow each line is deselected.

With the old revision manager the "deselect" process was under 1 min per pattern i think.

Is there a possibility to get the old revision manager active?

Is there a possibility to speed up the deselecting process?

I tried pack and go, but it grabs also the old drawings, which makes me more work in the rest of my process.

Greetings from Germany
Christian Kunkel
https://c-k-m.info
2 REPLIES 2
Highlighted

Re: Design Manager Performance issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have noticed issues as well and have had to log an IR on the issue.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Design Manager Performance issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not a fan of this new DM either. RM was much more robust IMO. Today I was doing a save as and you can"t browse to a location to set path?!

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200