Cancel
Showing results for 
Search instead for 
Did you mean: 

[Design Manager] Property manager?

Valued Contributor
Valued Contributor

In the old Revision Manager it was possible to access file properties both for solid edge files and for a whole folder. This last feature was very useful to add/modify/delete a custom property on all files in a certain directory, without the need to open the parent assembly. I'm unable to manage file properties for file and folder from Design Manager. File properties can be managed form Solid Edge, bot I don't find how to manage file properties for files in a folder.

 

Example: I have a folder with 100 draft files, and I want to add the same custom property to all. How to do this in Design Manager, coping and pasting from one file to all the other ones?

____________________________
http://www.stimarchetti.it
Design of automation
5 REPLIES

Betreff: [Design Manager] Property manager?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Alessandro

 

 

 

I think You are mixing up here something.

 

The global change of file properties for multiple files which are currently not opend IMHO only worked with Property Manager and not with Revision Manager

 

And using Property Manager still offers You the same functionallity

 

20170601_1250.PNG20170601_1251.PNG

regards
Wolfgang

Re: [Design Manager] Property manager?

Genius
Genius

Hi Alessandro,

 

You can stil do this, but only from within Solid Edge when you don't have any files open: Click the application button in the top left corner, then Info and then Property Manager.

 

Capture.JPG

Betreff: [Design Manager] Property manager?

Phenom
Phenom

@Alessandro is correct - In ST7 you can open Property Manager from Revision Manager.

Start Rev Manager and then click the application icon > Properties > Property Manager.

You can then open a folder full of files to modify.

The same applies in SE, but you do it before opening a file - once you have a file open in SE you only get properties for that file.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Betreff: [Design Manager] Property manager?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's still in Design Manager under the application button.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: [Design Manager] Property manager?

Valued Contributor
Valued Contributor

Many thanks to you and to all others that gave to me suggestions, and I apologize for answering so late, but I had a very busy day (BTW it is better to suffer for lack of time than the reverse! :-) ).

 

The solution was simple, may be I was "lost in transition" jumping from V18 to ST9!

 

Have a nice weekend!

____________________________
http://www.stimarchetti.it
Design of automation