Cancel
Showing results for 
Search instead for 
Did you mean: 

Design Manager

Valued Contributor
Valued Contributor
I am having trouble with Design Manager. I have created a fairly simple assembly with a sub-assembly inside of it. I built all of the parts using "Create In Place" in the assembly world. I have created the draft document, but now I want to move some of the parts into separate folders. I will leave the draft document and top level assembly in the upper folder. The sub assembly will get moved. When I try to "move" the parts in design manager using rename, not all of the parts get moved in the tree. This is not working as designed. I am in Ordered, ST9 Update 2. Is anyone else having problems with this?
2 REPLIES

Re: Design Manager

Phenom
Phenom

In general, when you're making assemblies with lots of interpart links, you're going to run into problems having those interlinked parts in different folders. Though I did notice an option in the Pack And Go function that preserves folder structure, I generally prefer to put any of the interlinked parts of an assembly all in the same folder. It saves you an untold amount of potential headaches if you do it this way, because if you have lots of subassemblies inside of a larger assembly, fixing the broken links if things ever move will drive some to suicide.

 

I would thank my lucky stars that I created the parts inside the same folder to begin with. I understand why you would want to organize in folders like this, I used to do that, until I really started seeing why it was a bad idea. Just my opinion.

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Design Manager

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

It is not necessary to keep parts with interparts in the assembly folder. Each part can be stored in an individual folder if you like. The interpart  links depend on the assembly where they were defined and not on directories.

When using interpart links in parts, you should not use these parts in other assemblies. In ST9 you will get a warning if you try.

 

Using the design manager ( revision manger for pre ST9 users) you can select the assembly and all contained parts at the same time, click the copy function from the ribbon and then the select directory function will set the new directory for all selected lines.

If parts contain interpart links, then these are updared to the new directory paths.

regards

JB
SE ST10