Cancel
Showing results for 
Search instead for 
Did you mean: 

Design/Revision Manager - Revise multiple files at the same time

Creator
Creator

One thing that I think is time consuming is when I want to revise multiple files at the same time.

 

For example, say that I have 10 drawings(and their parts) that I want to revise, I open all 10 drawing one by one in revision manager --> Set action to revise on both .dft & .par--> Perform action

Is there any better (=faster) way to do this?

 

When I release the drawings/parts after my changes I use life cycle assistant and there I can select all 10 drawing/parts and just change status to release, press next and finish and then I’m done. A much faster procedure then the one above.

5 REPLIES 5

Betreff: Design/Revision Manager - Revise multiple files at the same time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @stefan_s

 

 

at the moment I see only one quick and dirty method to do this and that might be to bring all the parts into an assembly (there is a macro whcih provides a one click solution for that) and from here YOu can start the DesignManager where again YOu can revise all parts and - a ST9 feature -  all according drafts in one step

 

 

 

 

 

regards
Wolfgang

Betreff: Design/Revision Manager - Revise multiple files at the same time

Creator
Creator

Okay, to bad there isn't a feature built in for that... But where can I find your macro? Smiley Happy

Betreff: Design/Revision Manager - Revise multiple files at the same time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Stefan,



I thought it was a macro by Klaus (incobase) but it isn't.

So I put the old version I have together with the readme into attached zip

 

Start the macro, select Your files and they will be inserted into the asm which still is opend .

 

Hope this is OK, but as I remember was it an open macro .

regards
Wolfgang

Betreff: Design/Revision Manager - Revise multiple files at the same time

Creator
Creator

Hi Wolfgang,

 

Thank you for the macro! It seems to work but I can't pick files from our manage insight server, only from different drives?

 

/Stefan

Betreff: Design/Revision Manager - Revise multiple files at the same time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@stefan_s, It likely isn't compatible with managed files.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200