Cancel
Showing results for 
Search instead for 
Did you mean: 

Design manager: how speed up for large assembly

Pioneer
Pioneer
Hi!
When I open Design Manager for a large assembly, It takes many minutes.
How can I Speed up It?

Thanks
20 REPLIES

Re: Design manager: how speed up for large assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm pretty sure it is what it is. No way to quicken.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Design manager: how speed up for large assembly

Legend
Legend

Opening ASM files and specially large ASM may take some time.

But... To be able to help you with your question, you should tell us a bit more details....

- How big is the ASM in part count?
- How much sub-levels are there?

- How is the folder structure?

- Are the files local or on a shared folder?

 

All this could influence the loading of the structure in DM.

 

--------------------------------------------------
Marc Boom
marc.boom@outlook.com

Re: Design manager: how speed up for large assembly

Pioneer
Pioneer
I check with the Asm with SE Reports:
-8500 different Parts
-9 levels
-we have a server with all files.
The structure is:
All articles are divides by type in many folders like:
C/.../tecnical/3D/pins
C/.../tecnical/3D/shafts
C/.../tecnical/3D/bolts
C/.../tecnical/3D/....
....
Many articles are assembly in their folders in their category.

And then, there are assembly where we put the articles together.
These assembly are in other folders
C/.../tecnical/3d/assembly/...

I have a full copy of this assembly in local, in 1 folder create with "Pack&Go" function, I can try to open Design manager from this, for test.
The time to open the assembly 3d, from server or from thiscopy is about the same, little less in local. I think that design manager is the same, but I Will test.

Re: Design manager: how speed up for large assembly

Phenom
Phenom

Do you mean 8500 total parts or 8500 unique (ie. different) parts ?

If its 8500 total I wouldn't consider that a particularly big assembly.

If you mean 8500 unique parts, what is the total part count ?

 

Your network speed and the number of users accessing the server will also have an impact.

In the past I've seen load times reduce considerably when I've been the only user accessing the server.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Design manager: how speed up for large assembly

Pioneer
Pioneer
I have:
1084 unique Asm
5699 unique par
1994 unique Psm

Many of these files are repeat, and the total pieces are:
3987 Asm
24448 par
9905 Psm

Re: Design manager: how speed up for large assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yeah, that's huge.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Design manager: how speed up for large assembly

Legend
Legend

@Cek

Hello,

well sorry but we have here more par and more asm and see no point how to get it faster done.

good luck and let us please know your results.

 

Best Regards

Wolfgang

Re: Design manager: how speed up for large assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

You have a copy on your local drive that has similar performance results.

 

On this test data, have you run OpenSave on everything?  I just wonder if a lot of time is being spent resolving out of date links.

Re: Design manager: how speed up for large assembly

Pioneer
Pioneer

Hi! @uk_dave

I don't run OpenSave utility.

I try 1 time for another test of a similar big assembly, copied in local, but the program crash after about 1000 files.

I don't know the utility of the OpenSave of all files, but I read that is a good job to do.

 

I run the SESysInfo with the assembly and there are a lot of unused file .jpg (texture), but not missing files. (because a lot of files are created with previous version of solid edge and they are search in texture folder by the previous version of SE).

I searched an app for repair this unused links but I don't found it.

I can try to run OpenSave in a copy in local and then try open Design Manager and the assembly.

 

We also have a lot of time with open all the assembly (it takes 10 minutes) but with configuration and the options for large assembly we redused a lot time. But remain the time problem with the Save and the refresh/update assembly. They takes a lot of time. (I check the options of Refresh and Save limites to only the modified files, but there isn't a good speedup).