Cancel
Showing results for 
Search instead for 
Did you mean: 

Dialogue Box

Valued Contributor
Valued Contributor

Using ST8 and occasionally the dialogue boxes disappear and you have to click on the SE window to get them to appear. Shutting down and restarting SE cures this issue. Is it a graphics card problem and does anyone else see this? It used to happen in previous versions too.

Thanks

 

Graham

3 REPLIES

Re: Dialogue Box

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Which dialog boxes are you referring to redcad ?

 

~Tushar

Re: Dialogue Box

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Graham,

 

Not seeing this here....

Is it all dialogues in general, that loose focus?....or is it only specific ones??

 

Could you capture & post a video of the occurance???

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Dialogue Box

Valued Contributor
Valued Contributor

I'm not sure what causes it but it is all dialogue boxes. It doesn't happen all of the time just occassionally. I've had it happen in previous versions and on previous PCs/graphics cards.

 

G