Dim edit in draft

Honored Contributor
Honored Contributor

Is there a way to change/edit what object and existing dimension is attached too? If I could edit where one end of a dimensions is going, it would save me some time.

 

Rather than go into details, there are downstream calculations resulting from the variable assigned to the dimension. If I delete and replace, I have to fix all the downstream calculations.

3 REPLIES

Re: Dim edit in draft

Esteemed Contributor
Esteemed Contributor

Select the Dim, hold down ALT key, drag dim reference line handle to new element.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Dim edit in draft

Phenom
Phenom

I know this has been answered, but a little more information doesn't (usually) do any harm.

I'm not sure if you do this, but I find it best to create my own variables and apply values to them, do the calcs on those variables and then link them to dimensions. This way the calculation is not lost, only the link between a dimension and the variable, which can easily be re-applied.

If you do calculations based on dimension name you could lose both.

 

Example -

dim A = Dim B x Dim C

 

create variables a, b & c

assign values to b & c

assign formula b x c to a.

 

dim A formula = a

dim B formula = b

dim C formula = c

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Dim edit in draft

Phenom
Phenom

Such tips are welcome, since they teach something beyond the realm of the just CAD.

This is surely a 'Best Practice'.