Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dimension Scale Wrong when use Control vertex relation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi all;

I have promble when put dimension on point. This point create form Control vertex relationship. The promble show when I change Drawing Scale 1:1 to 1:2. Dimension is scale too. Please in attach file.

How I fix this dimension?

12 REPLIES 12

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

 

due to the fact that we do not have the original draft file for verifying, I only can assume following:

 

You have created Your point on paper space rather than inside the view.

 

So Your dimension point from an element on paper (scale 1:1) to an element from a drawing view with a ceratin draft scale.

If this draft scale is 1:1 everything is OK.

But if You have a different draft scale and Your dimension was created starting from the point on paper the dimension scale insied is 1:1 and stays 1:1

 

This was a common behaviour of Solid Edge in former versions.

So I also only can assume that You are not on current version of Solid Edge

 

Doesn't matter anyway.

 

The correct prcoedere to handle such a task is to use the "Draw in View" command on the RMB (Right Mouse Button) over an draft view.

 

Inside the view You then create Your helping elements - suggest to use a small circle rather than a point (it is seen better and You can use the C command for center)

 

And do not forget You also can use the "Intersection method to get it right!

 

 

I will create a short video and upload within the next minutes.

 

 

 

regards
Wolfgang

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

and here is the promised video showing the "Draw In View"

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

regards
Wolfgang

Betreff: Dimension Scale Wrong when use Control vertex relation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Perfect!! Thank you. but not have any way for fix this? Haha.

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

sorry for not understanding Your answer.


Famer schrieb:

Perfect!! Thank you. but not have any way for fix this? Haha.


 

 

Can You please explain this for a non native English speaker?

Thanks

 

 

regards
Wolfgang

Betreff: Dimension Scale Wrong when use Control vertex relation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I can download this video?

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Famer

 

 

the inplace video should be possible to view with a simple click on the play button.

No download etc.

 

Maybe this has to do with Your browser, setting, operating system etc.

 

 

 

regards
Wolfgang

Betreff: Dimension Scale Wrong when use Control vertex relation

Experimenter
Experimenter

Hi, "Use draw in view" has nearly solved my issues of dimensioning construction lines placed over a model view and keeping the right scale......however when I dimension in "draw in view" and then switch to sheet view, the dimension lines are way off where I placed them, and can't be edited from sheet view! Any solution?

JP

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @JPac

 

 

my suggestion for this will be: "To not draw this in a draft view and dimension it!"

 

Just do it in 3D document as a sketch.

You can retrieve (show) this sketch in draft too, together with all dimensions as YOu need them.

And - important - once You have created this sketch You always can us it together with that part without the need of repeatiing the same work again and again.

 

And geometry is associative and usable in part too.

 

regards
Wolfgang

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @JPac,

 

We often use the "Draw in View" function here, to show situational information that we don't want in the 3D model,  and when placing dimensions, they [and some other sketch geometry] are always placed on the "Auto - Hide" layer, unless we forget, and have to go back in and use the "Move Elements" command.

 

 

ST10_DFT_DrawInView_Dimensions [Auto - Hide].PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000