Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Dimension Scale Wrong when use Control vertex relation

Experimenter
Experimenter

Great, thanks, that's solved it - just one weird thing is that the lines from the part sketch look different in draft view - some come as dotted, some as solid, no matter what they are in the original sketch.....

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@JPac, strange alright......could you post a screen capture of both, to better see what is going on? As I'm wondering if it could just be screen scaling, and not the actual geometry. Just a thought.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: Dimension Scale Wrong when use Control vertex relation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @JPac

 

 

 

sketch elements also are proceeded as any other edge elements.

Visible, hidden, etc.

 

But You can define any line type to the complete sketch if wanted.

 

regards
Wolfgang