Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension Styles in Callouts

Valued Contributor
Valued Contributor

Does anyone know if it's possible to have more than one dimension style in a callout?  Specifically, I'd like to call out my drill thru and c'bore diameters fractional, but have my c'bore depth a three place decimal.

 

Thanks,

 

Matt

4 REPLIES

Re: Dimension Styles in Callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't think so. I was going to suggest that maybe you could use a dual unit display but callouts are apparently incapable of that.

I consider your request a little odd but I would think dual unit display should be possible but it looks like you can only make it work on the selected entity's dimension. For example, on a counterbore, dual unit only works on the inner or outer diameter (depending on which you select). And forget about depth.

The dual unit setting doesn't apply to the text string modifiers in the dimension prefix or feature callout dialogs. Those are what callouts use.

You'd have to use two dims or callouts to do what you want.

MultiUnitCallout.JPG

 

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Dimension Styles in Callouts

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

bshand is correct.

 

This isn't a odd question cause this go's back many many many years. Some of us requested for this typ of behavior for call outs, different units in one callout. Not sure if there's still a ER out there for this. If i have a c'bore that needs to be 3 plcs and the other are fraction, i'll show it in a side view. 

Re: Dimension Styles in Callouts

Valued Contributor
Valued Contributor
Thanks everyone.

Re: Dimension Styles in Callouts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TDB, Thanks for correcting me on the "oddity". Because I've never needed it makes it odd to me I should have said. I suppose there are times where depth could require tighter tolerances than the diameters. Whether you use decimals or specify smaller fractions for the depth tolerance is discretionary I suppose.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200