Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension lines

Experimenter
Experimenter

I just need someones knowledge on how to change the lines on the dimensions so that the two end lines don't actually touch the lines of the drawings. I would like them to have a gap.

i'm sure this is possible to change but i just can't find out how to do it...

have attached a example of how it automatically does it now.

 

thanks in advance.

1 REPLY

Re: Dimension lines

this should happen auto"magically" when placing dimensions IF you select near the end point or the endpoint of the line.

 

To edit this after the fact: select the dimension, note the anchor points where the extension lines attach to the drawing view,  while holding the ALT key, click and drag the anchor to the endpoint of the line.  this should then envoke the dimension style and use the default

 

moveanchor.png

element_gap.png