Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension problem when scaling

Creator
Creator

I am trying to dimension the distance of a cut out:

 

First.PNG

The dimension I wish to change is the .793.

 

 

Second.PNG

 

 

 

I change it to 1.0, but this happens:

 

Third.PNG

 

The line above it says it is "Not in Scale", what ever that means.

Why can I not change that dimension?

 

Alfred

3 REPLIES 3
Highlighted

Re: Dimension problem when scaling

Gears Phenom Gears Phenom
Gears Phenom

 

try to click the vector arrow on the dimension so that the anchor in the axis and the aarrow points to the cut depth... ?

 

if you want to share your part file we would be happy to take a closer look and advise...

 

 

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Dimension problem when scaling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @alfred

 

 

 

as already mentioned by @Johnson_BigMatt the best always would be to share the part, but as far as I can see on Your pictures, there is a small red cross on the left side of the cutout.

 

This is the symbol for a connected relation to - I suppose - the center, axis, sketch, etc. - and this will prebent You from any movement of that side face.

This assumption will be forced by the brown line what also indicates that You tried to change something what can't be changed

 

Try to delete that and I think everything will work fine.

 

 

regards
Wolfgang

Re: Dimension problem when scaling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@alfred  It appears you are using the Ordered environment.  As such, the Dimensions need to be "locked" to drive the geometry otherwise you just override the label hence the underline.  When you click your existing dimensions, notice the "unlocked" lock button on the dialog.  Click it to "locked".

 

When placing a new dimension, there is a lock on the Command Bar.  Make sure that is "locked" before placing the dimensions and then you will not have to lock them one by one.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com