Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension to intersection

Valued Contributor
Valued Contributor

How do to select the intersection of these two lines (black lines)? 

do i need a add a point first, where the intersection lies. 

 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
6 REPLIES 6

Re: Dimension to intersection

Genius
Genius

see attached video to verify the option is turned on.

then hover over the first line, then move over and hover over the section.  

next move the intersection point.  the item will appear.  left click and then move to final dim. pick point

Cory M
Solid Edge ST10
ST10 Cert

Re: Dimension to intersection

Valued Contributor
Valued Contributor

Hi,

 

you don't have to add a point.

You should move the mouse over the first line and then the second one. Then move the mouse approximately to the intersection. When the cursor change, click LMB. See the attached video.

In my opinion sometime very difficult to find the intersection, because I have to estimate "by my eye" where is the intersection point. I would also like to know about a better solution.

I hope somebody know about a switch somewhere, which show all of the intersection points on a view Smiley Happy

SE2019 MP3

Re: Dimension to intersection

Genius
Genius

It depends on what you are trying to do.  If you are adding a line or sketch element, you can hove over the two lines and then find the intersection.  If you are trying to dimension to the Theoretical Sharp Corner, you may need to insert a point.  See video below.

 

EDIT: My response is for the part environment but it looks like you were seeking an answer in Draft which has been addressed in previous posts.

 

(view in My Videos)

Brian Fritz
Solid Edge Certified Professional
ST10 latest MP

Re: Dimension to intersection

Valued Contributor
Valued Contributor

@cmaxwell thanks for that, yes i had that option on in IntelliSketch  but realised i was dimensioning it incorrectly. 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Dimension to intersection

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Don't forget about MICE keystrokes.

Mid

Intersect

Center

End

LMGi
www.TLMGi.com

Re: Dimension to intersection

Gears Phenom Gears Phenom
Gears Phenom

https://grabcad.com/tutorials/how-to-better-select-keypoints-for-dimensioning-in-solid-edge

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7