Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension to the top of an arc?

Valued Contributor
Valued Contributor

How can i dim to the max point of this arc.

In SW im used to use the min max options , where can i find this in SE?

 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
2 REPLIES 2

Re: Dimension to the top of an arc?

Gears Phenom Gears Phenom
Gears Phenom

use the distance between tool and select tangent

 

2-16-2018 6-40-17 AM.png


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Dimension to the top of an arc?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Johnson_BigMatt

Hi @MagRiz

 

 

You also can use the Smart Dimension to do so. 

 

Tangent Option or "T" always is available to be activated 

 

 

regards
Wolfgang