Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension tolerance size difference ST7

Genius
Genius

I have a series of drawings that have minor differences, mostly lead wire length. I have elected to use a common model for several drawings.

 

When I set Dimension Type to Blank and enter needed dimension in Prefix field, I do not see an option to set the tolerance size to match the normal dimension tolerance size of x.70 font size. Is there a way to do this or some work around solution?

 

In attached screen capture the 795 ±15 and 40 ±2 are manually entered dimensions, the 3.5 ±0.5 is a standard dimension.

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

1 REPLY 1

Re: Dimension tolerance size difference ST7

Legend
Legend

Set your tolerences via the unit/alpha tolerence as normal and just set the dimension to "not to scale" and type in the major dimension number.