Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimensioning Rounded Radii

Experimenter
Experimenter

I am trying to dimension a bean shaped part that has two different radii. One is set from the center point, while the other is set .225 inches away from the center point. My problem is that the bean shape is extruded, drafted at 5 degrees, and rounded at a radius of 0.016. When the rounded radii are suppressed, the bean radii are correct and snap to the correct points, but when the bean is rounded the bean radii are off by 0.001. Is there a way to get the true radii values while the bean is rounded?

 

The values of R. 0.237 and R. 364 are the correct values I am trying to achieve.

 

 

6 REPLIES

Re: Dimensioning Rounded Radii

Gears Phenom Gears Phenom
Gears Phenom

I don't support you can upload the part file without violating and intellectual property or export rules?


____________________________________
--Scott Wertel, P.E.

Re: Dimensioning Rounded Radii

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The edge that you have without the round is not there when rounded as there is no "Edge" geometry there to dimension to.  Because of the draft, when the round is applied the edge moves slightly down the drafted face therefore the dimension you see when it is rounded is the correct radius.

2016-06-27_15-01-07.png



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Dimensioning Rounded Radii

Experimenter
Experimenter

Is there a way to pick up that virtual edge in a drawing or is the the only solution to leave the rounding off?

Re: Dimensioning Rounded Radii

Valued Contributor
Valued Contributor

In your draft, you're likely dimensioning to tangent edges instead of the actual radii.  A tedius solution would be to project an outline sketch onto a plane above the feature before adding the corner radii and drafts.  You can then show and dimension to the sketch on your drawing.  A section view might be a bit easier.

 

It would sure be nice if Seimens could develop a view option to overcome this.  The software can calculate a tangency, why not a theo. sharp corner.

 

Good luck.

 

Matt

Re: Dimensioning Rounded Radii

Phenom
Phenom

I would create a section and dimension to the intersection as shown in Ken's sketch.

It would be much clearer that way.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Dimensioning Rounded Radii

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Other option would be to create a Simplified part rep with rounding removed.  You can then place a view of the Simplified version in your Draft as well.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com