Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimensions Error

Experimenter
Experimenter

 

 

Access to disappear during the dimension edit profile.

 

I have a lot of similar types of problems.

 

help me.please

 

I can't fix it.

 

 

edge st 6

 

k620 quardro

 

 

10 REPLIES

Re: Dimensions Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm guessing your issues are related to your graphics card.  I would insure you have the latest driver for it installed.  If that doesn't work, you might try disabling the "Automatic selection" setting in the Application Display area of the Options and then set the setting to "Backing Store".

 

Are you also running the latest Maintenance Patch for ST6 (MP 14)?



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Dimensions Error

Experimenter
Experimenter

my graphics card is k620

 

driver version : 362.56

 

'Backing Store' is very slow 

 

`Are you also running the latest Maintenance Patch for ST6 (MP 14)?`

   Yes

 

Re: Dimensions Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Daeho,

 

Could it be the OS?.....what operating system are you running??

 

nVidia list a newer driver version "368.39" for the K620.....maybe give that a shot.

 

http://www.nvidia.com/download/driverResults.aspx/103904/en-us 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Dimensions Error

Experimenter
Experimenter

Hi SeanCresswell

 

my os is window7 64bit

 

also.. I did update 368.39 but i have same problem.

 

thanks

Re: Dimensions Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Daeho,

 

Well that's no good......I was kind of hoping to pin the blame on ST6 in "Windows10".  Robot Frustrated

 

Could it be a loose connection in the hardware?

 

If you're comfortable with it, [seek IT help if not] try a de-couple & re-seating of the graphics card, and if the issue still remains,....then try the same thing with all system memory [RAM] modules.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Dimensions Error

Experimenter
Experimenter

I did reassembly today. Robot Sad

 

 

edge : st6 mp14

 

os : win7 64

 

cpu : E3-1230V5 

 

 

vga : k620

 

ram : 8gb

 

 

Re: Dimensions Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure where to go from here.  Do you have anyone who can log into that PC with a different user account and try it?  Sometimes a user profile in Windows will get some kind of corruption that causes wierd issues, but it is rare.  Easy to identify that as an issue by having another login account try the same in SE.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Dimensions Error

Experimenter
Experimenter

give up....

Re: Dimensions Error

Phenom
Phenom

Since going forward with the driver isn't helping how about if you install an older driver?