Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimensions auto-populate/create?

Legend
Legend

Just got to thinking: when I draw a circle, line, or rectangle, I have to enter dimensions, why do I have to go back and add that same dimension? Why doesn't it auto-populate/dimension the same way I built it?

 

Just seems a little weird to enter dimensions twice.............build a rectangle from center, put in the dimensions I want, and then I have to go back and dimension those same lines.

4 REPLIES

Re: Dimensions auto-populate/create?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can do this.  Use Command Finder and search for "Auto Dimension".



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Dimensions auto-populate/create?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

AUTODIM.JPG

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Dimensions auto-populate/create?

Legend
Legend
SPECTACULAR!

Re: Dimensions auto-populate/create?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,

Hi @bshand

 

 

I also like and use this function for years, and this is my personal preference I set the option to 

"Only when geometry is created with keyed-in value"

 

So when sketching geometry without enter any dimension nothing will be different than the behaviour You always had and Your are used to have.

 

But if You type in any value for a geometric element the according dimension will be ceated immediately

This saves time but doesn't produce unnecessary elements.

 

regards
Wolfgang