Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dimensions

Valued Contributor
Valued Contributor

Great that you can stack dimensions, but if i try to do a chaindimension, upon previous plaxced dimensions, it won't work.

see jpg

5 REPLIES 5

Re: Dimensions

Legend
Legend

Did you use a "Distance Between" dimension and click on the dimension you want to chain to as the first move?

Using SE since V12, 2002
ST10 certified

Re: Dimensions

Valued Contributor
Valued Contributor

yes

Re: Dimensions

Legend
Legend

I assume you are using ST6. I just started that and the associative dimensions have changed. If SE thinks the previous dimension is stacked it will keep making it stacked. Try picking the dimension you don't like and hold the alt key down and drag the attachment point to the place you want it to be. Then hold the alt key down again and drag the dimension line to line up with the correct dimension. It should all lock together.

Using SE since V12, 2002
ST10 certified

Re: Dimensions

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

There is a PR filled for this and there working on it. I was hoping to see something soon

Re: Dimensions

Creator
Creator
I have facing same issue for chain dimension..is there any update..?