Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimensions

N/A
Hello,
how to place dimensions that not shuld be horizontal oder vertikal?
for example the true distance between the two points A and B
+
A \
\
\
+
B

regards

Robert
2 REPLIES

Re: Dimensions

N/A
Choose smart dimension, click on the first object, then click on the second object then press and hold shift, you will see the dimension will change from vertical/horizontal to aligned. Kind Regards

Extra note: You can also put the two items on a circle (with the radius set to the distance you want them apart), and put the circle on the Auto hide layer so its not shown in your sheets.

Re: Dimensions

N/A
You can also use the Distance Between dimension type.
There is a combo box when you run this command where you set the alignment.
Change it from 'Horizontal/Vertical' to 'By 2 Points'.
Regards,
Rick B.