Cancel
Showing results for 
Search instead for 
Did you mean: 

Dims issue question

Gears Phenom Gears Phenom
Gears Phenom

Hi all,

 

I have got a question regarding to changing dimensions by adding extra value as shown on the video.

 

Is there a different method to avoid removing 'mm' suffix ?

 

Thank you,

 

Arek

(view in My Videos)

3 REPLIES 3

Betreff: Dims issue question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



there only is an option in SE settings to avoid units generally.

You find that under options - general and just at top of the tab You see "Show units ...."

 

20161010_1009.PNG

 

 

Set this off will avoid units within dim fields

20161010_1010.PNG

regards
Wolfgang

Re: Dims issue question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @arekkul,

 

If you don't want to remove the units from the fields, you could try editing the formula of the dimension.....right click the dimensions to get that option.

 

Here's a quick video....

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Dims issue question

Gears Phenom Gears Phenom
Gears Phenom
You are the Stars !!!!

thank you,

Arek