Cancel
Showing results for 
Search instead for 
Did you mean: 

Disable auto revision triangle

Valued Contributor
Valued Contributor

Where in the options can i turn off auto rev triangles on drawings?

Regards,

MagRiz
(ST9 User Est 01.18)
2 REPLIES 2

Re: Disable auto revision triangle

Gears Phenom Gears Phenom
Gears Phenom

You will find this as an option within "Track Dimension Changes" 

 

The tool is designed to show you what changed and then you can 1 by 1 review and/or you can simply clear all...

 

But if you do not want to track changes you can the options to turn off track changed dimensions.

1-30-2018 9-21-10 AM.png1-30-2018 9-21-49 AM.png

 

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Disable auto revision triangle

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

see picture from Draft Dimensions Tracker:

 

20180130_1524.PNG

regards
Wolfgang