Cancel
Showing results for 
Search instead for 
Did you mean: 

Disappearing cross-hatching in draft.

Phenom
Phenom

When I create a section view in draft the cross-hatching appears OK.

If I then set a display depth on the section the cross-hatching disappears.

Any ideas ?

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.
2 REPLIES 2

Re: Disappearing cross-hatching in draft.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Are you placing the depth line beyond the section line / cutting plane ?

 

Re: Disappearing cross-hatching in draft.

Phenom
Phenom

Yes, the depth definition is correct.
I thought maybe it was because the depth extent was closer to the cutting plane than the end of the part, but it is not consistent with that.
I also find that some parts still hatch correctly.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.