Cancel
Showing results for 
Search instead for 
Did you mean: 

Disappearing parts

Phenom
Phenom

Hi All,

 

have you noticed in SE ST9 the disapperaed parts in the assembly mode ?

 

When I want to activate the part it is disappearing...

 

thank you,

 

Arek

5 REPLIES

Re: Disappearing parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have not, but I would suspect graphics card/driver.  What graphics card do you have, and are you using an updated driver?



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Disappearing parts

Honored Contributor
Honored Contributor

I would suspect the graphic card as well. I don't get that problem but what I do get is:

 

When the vid card is no longer able to clean up it's ram (I call it out of gas), then I can no longer select sketches for extruding or whatever. I can see it, but not select it. Very frustrating. Typically I have to reboot the computer every 3 hours to remove the problem. 

 

I use  K4200 Vid card.

 

In the reallly big picture. This is from Nvidia's drivers. Nvidia stole the good bits of code from 3Dlabs and have never implimented them 100%. Some version of drivers for each card have different problems then others.

Re: Disappearing parts

Phenom
Phenom

Thanks Dudes for very quick response,

 

I faced this issue after my SE ST9 crashed. I believe thi is not a graphics, but maybe I am wrong.

 

I am having N Quadro 4000 with the driver ver. 10.18.13.6256 ( driver date: 10/05/2016 ).

 

regards,

 

Arek

 

 

Re: Disappearing parts

Valued Contributor
Valued Contributor

suspect the graphic card !! share the assembly if possible .... Forum guys can check it for U .. Smiley Wink

MfG -
Viv

Re: Disappearing parts

Valued Contributor
Valued Contributor

We are seeing the same thing.  Dell Precision's 71700 with Nvidia K4000 cards.  I doubt it's the cards seeing as this is ramdom.