Cancel
Showing results for 
Search instead for 
Did you mean: 

Distance Between in ST5

Creator
Creator

I'm trying to move a line in a part that I'm drawing using the distance between command.  The line won't move and I've never run into this problem.  I was wondering if someone out there could point me in the right direction?  Thank you very much.

6 REPLIES 6

Re: Distance Between in ST5

Phenom
Phenom

Could you please upload your model? Which line exactelly do you mean?

I'am using ST5 too.

 

Yasser

SE STx

Re: Distance Between in ST5

Creator
Creator

Thank you very much for your response.  It is the vertical line just below the through hole.  We are trying to shift it to the right but it is locked.  Not sure if it is something in the settings or our process is incorrect.  Thanks again.

 

 

Re: Distance Between in ST5

Phenom
Phenom

I can't open your ST5 File!

 

Are you using an academic version?

 

Yasser 

Re: Distance Between in ST5

Creator
Creator
yes we are

Re: Distance Between in ST5

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The vertical line is perhaps connected to the horizontal line below it.

 

2015100101.png

 

You can turn Relationship Handle display ON and see if there is a Connect relation at the end points.

 

2015100101.png

Re: Distance Between in ST5

Creator
Creator

That Worked!!!!!  Thank you very much.