Cancel
Showing results for 
Search instead for 
Did you mean: 

Do not appear the solid models! in Solid Edge ST5

N/A
Hi Kris:

Thanks a lot for the Trial Version of SE ST5.
I have a problem. I cannot see the solid models that I created following the first exercise. I do not see the arrows of the coordinate systems either. I went to the show menu, and checked on the different options, but nothing happens.
what can be the problem.
Since I have not advanced more than that, I do not what else can be missing.
I did not see anyone posting a message on this topic.

I hope you have a chance to see these problems.

Thanks for your attention. Jose Saldivar.
1 REPLY

Re: Do not appear the solid models! in Solid Edge ST5

Pioneer
Pioneer
Is there a chance the model is simply out of the view? Did you try to use the Fit command on the view tab to see if the model is actually there? Also in the PathFinder to the left, do you see the list features you created to build the model?