Cancel
Showing results for 
Search instead for 
Did you mean: 

Document change in par file

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Haven't dug in to it but, is there a way to document the changes you've made in the par file? One of our tool supliers is asking about it. plus, supposaly Pro E can do this....what ever...Smiley Happy

4 REPLIES
Highlighted

Re: Document change in par file

Phenom
Phenom

There isn't a notes function as such, but a good way of doing it would be to use the PMI tab functions. With those you can do a text callout with arrow to note a change to a feature or add dimensions etc. 

I don't know if you're using PLM, but some programs will allow you to add notes to a dataset or similar.

Re: Document change in par file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There's a "comments" property.

Also you could embed a Word document, text file or whatever with the binder function.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Document change in par file

Siemens Phenom Siemens Phenom
Siemens Phenom

My understanding of the Pro/E track changes tool is that it is only for the current session -- it does not  permanently stay in the file:

 

http://support.ptc.com/appserver/wcms/relnotes/note.jsp?&im_dbkey=130984&icg_dbkey=826

 

Re: Document change in par file

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Thanks all for a couple of ideas. i'm personaly not pushing this since we document everything on our dft. majority of the time the dft/pdf go's along with the par file

 

Thanks again