Cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST9 work in Windows 10 Home Edition?

Experimenter
Experimenter

Hello,

I have Windows 10 Home Edition and I can´t run the ST9 version (server error), do I need ST8 version?

And if it is so, where can I download ST8 version?

Thank you in advance.

5 REPLIES

Re: Does ST9 work in Windows 10 Home Edition?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't see why it wouldn't work but Windows Home is not supported.  Do you happen to have the 32 bit version of Windows 10?  SE id a 64 bit app and will not run on it.

 

If ST9 won't work, doubtful ST8 will as it has the same system requirements.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Does ST9 work in Windows 10 Home Edition?

Experimenter
Experimenter

Thank you Grundey  for such a quick response.

It seems that the problems is another program (antivirus,...).

Thank you.

Re: Does ST9 work in Windows 10 Home Edition?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And when you install, right mouse click on the Setup.exe and select "Run As Administrator" if you aren't.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Does ST9 work in Windows 10 Home Edition?

Experimenter
Experimenter

hi Ulhi,

facing the same, or a similar problem - this window comes up everytime I want to install, also with all anti virus switched off.

image.png

How did it eventually work on your end?

thanks 

b.

 

Re: Does ST9 work in Windows 10 Home Edition?

Siemens Phenom Siemens Phenom
Siemens Phenom

The issue is exactly the message being displayed -- your installer file is corrupt.  You will need to re-download the installer file again.  When downloading, use a download manager to control the download.