Cancel
Showing results for 
Search instead for 
Did you mean: 

Dotted alignment lines gone

Experimenter
Experimenter

Hole alignment.  In the past when I created one circle I could move to the left or right, or up or down and a dotted line would show me that I was aligned with the first circle when placing the second.  That functionality seems to have disappeared (I'm sure I turned something off - don't know what).

 

Along those same lines a behavior I'd like to turn off is when doing what I describe above that dotted line seems to want to snap to every point in the drawing.

 

I would appreciate any help anyone might offer.

 

Thanks,

 

Len

3 REPLIES 3

Re: Dotted alignment lines gone

Experimenter
Experimenter
Oops. ST8 2D

Re: Dotted alignment lines gone

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Len1

 

 

 

sounds as You have turned off the "ident idicator" in draft

 

See the pictrue and I hope this is the reason

 

20161126_0841.PNG

regards
Wolfgang

Re: Dotted alignment lines gone

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Len1

 

 

besides the above function see that indicators are kept and shown too:

 

20161126_0842.PNG

 

 

regards
Wolfgang