Cancel
Showing results for 
Search instead for 
Did you mean: 

Dowel hole symbol

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hello,
When I create a dowell hole in part env, I need it to be show the dowell hole symbol during detailing.
Kindly help.
Thanks.
Regards,
Ashish Sarode
9 REPLIES 9

Re: Dowel hole symbol

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Ashish:

 

In the draft, you can hide edges and replace them with a block of the dowel symbol.

 

~Tushar

 

Re: Dowel hole symbol

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hi Tushar,
Thanks for the reply
Can you send me a video demonstrating it.

Re: Dowel hole symbol

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Ashish:

  

Here's how the removed edges replaced by a dowel pin symbol will look like (see attached):

Let me know if the output is OK for you; this is not something that I have practiced, but only an idea that came to mind. I will make the video and post shortly. I have ST 9 beta on this PC and don't think can post a video using it for another week. I will access another PC with ST 8 to make the video.

  

 

 

 

~Tushar

Re: Dowel hole symbol

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

If i understand correctly. all you to do is go in backgound and hatch the hole. draw lines for the area to hatch. this is the only way i know how

Re: Dowel hole symbol

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This approach by @TDB is a much cleaner and practical one.

As I said I have never practised it but just an idea that occurred to me.

 

Re: Dowel hole symbol

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Siemens is once again behind the curve on this. They should provide the proper symbology in SE like cousin SW.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Dowel hole symbol

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Ashish:

  

Here's a video about TDB's solution:

https://app.box.com/s/vo2wzm4unmtjr5nx0990kx2x2jypcjgb

  

The advantage with this method is the symbol will scale with the view.

  

~Tushar

Re: Dowel hole symbol

Phenom
Phenom

Booo, Bruce!

SW only has that function for hole wizzard holes. Otherwise the manual option is the same thing- a fancy sketch that is "attached" to the hole diameter.

Re: Dowel hole symbol

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

? Hole wizard holes would be good enough. Certainly better than nothing. We're talking about holes, right? Well, we're talking about pins too, but the machinist is concerned about hole placement.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200