Cancel
Showing results for 
Search instead for 
Did you mean: 

Download link for 2D Drafting ST6

Experimenter
Experimenter

Can someone give me a link to download a free version of 2d drafting ST6 as i only have a 32bit pc.

 

Ive tried  couple of links on this forum but one requires a webkey which i dont have and the other requires a licence which again i dont have.   Thanks..

7 REPLIES

Re: Download link for 2D Drafting ST6

Experimenter
Experimenter

44 views and no replys, cheers fellas. guess i'll have to use an alternative

 

Seems a bit daft that siemens doesnt give the option to download the older ST6 version for us folk who only have 32bit pc's

 

I even contacted them about it and all they sent was a link to this forum lol............

Re: Download link for 2D Drafting ST6

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You might have had better luck posting in the right forum category for this at... http://community.plm.automation.siemens.com/t5/Solid-Edge-2D-Drafting-Forum/bd-p/SolidEdge-2D-Drafti...

 

 

As with (I presume) other USERS here, they probably read the part where you're locked into a 32bit PC, and realise there is not much we can do to help.

While you might get lucky, and have someone from Siemens to offer you a link to the outdated version, I wouldn't be too expectant.

 

Have you considered getting an upgrade to 64bit Windows?....would seem rather critical to the ongoing use of Solid Edge.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Download link for 2D Drafting ST6

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@Jay998 wrote:

I even contacted them about it and all they sent was a link to this forum lol............


You sure were directed to the right place - this forum.

@SeanCresswell and the gang out here are the Level-III support after VAR and GTAC !! Man LOL

 

~Tushar

 

Re: Download link for 2D Drafting ST6

Phenom
Phenom

Not sure if this is possible, but can you still get ST6 full download?

You might then be able to get a ST7 2D drafting license to use with it.

 

Edit: Just been on GTAC site and ST6 32bit is still available for download.

(Full licenses are usable with previous versions, so maybe the 2D is also.)

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Download link for 2D Drafting ST6

Experimenter
Experimenter

I also only have a 32Bit computer.

Can someone please give or send me a link to download the ST6 2D Program?

Thanks.

Re: Download link for 2D Drafting ST6

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Look at your private message box! Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Download link for 2D Drafting ST6

Experimenter
Experimenter

Hello, I need Downl. link to 2D drafting ST6 too, please. It is impossible to get.

Thanx a lot for your help... Rado.