Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Download server of ST8 student editons is extremaly slow

Experimenter
Experimenter

What is going on with ST8 Student Edition download server? Despite my 50Mbps connection, ST8 install package initial download speed is 350 kbps and then it slows down linearly, and in some point download fails, causing error. Is there any mirror for ST8 installation? Or can I download trial, and enter student's licence number?

1 REPLY 1

Re: Download server of ST8 student editons is extremaly slow

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Arct,

 

 

Just a thought.....you might consider, depending on where you are physically located, is contacting a local Solid Edge reseller [even another user], and asking for a copy of the installation file on a flash drive, or DVD......as it is only the license file that is unique, and activates it as the Student Edition.

 

 

FYI: my connection speed floats between 500~700KB/sec [not even kidding] and it sticks with it until completion just fine....are you using a download manager? [highly recommended]

 

Capture.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000