Cancel
Showing results for 
Search instead for 
Did you mean: 

Downsizing a Object

Experimenter
Experimenter

Hello, I am trying to 3D Print a Cow, the file I have the cow is 125" long I would like it to print it about 6" long. Is there a way to shrink the whole cow?

Thanks

2 REPLIES 2

Betreff: Downsizing a Object

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @aaronw1 

 

 

 

You can use the scale function of SE:

 

20190517_1956.png

regards
Wolfgang

Re: Downsizing a Object

Legend
Legend

Hi,

 

You can use the command " insert part copy" in the part environment.  

 

You can set the scale, and scale it down, uniform or in one axis... creating a very, very long cow... 

 

Regards,

 

Jan Bos

Emmen, the Netherlands