Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft: Change size of centermark?

Valued Contributor
Valued Contributor

Hi again Smiley Happy

 

Do you guys know if it's possible to change the size of a centermark? I find it rather big.

4 REPLIES 4

Re: Draft: Change size of centermark?

Valued Contributor
Valued Contributor

I can right-click and choose Properties, but that is not used as default.

Is it possible to change the default size?

Re: Draft: Change size of centermark?

Valued Contributor
Valued Contributor

I found it Smiley Happy

 

View ribbon -> Styles -> Lines and Coordinates -> Center Mark = 2 x fontsize

Re: Draft: Change size of centermark?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


congratulation for finding the option before any answer solved that.

 

But IMHO the 2 times text size could be to high too.

I prefer 0.5 times textsize, so that the center marks are appr. 1.5 mm 

 

 

regards
Wolfgang

Re: Draft: Change size of centermark?

Valued Contributor
Valued Contributor

Will try that, I kinda found it a bit too big too, even at 2x text height.

So many possibilities in this software Smiley Happy