Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft: Rotate views

Valued Contributor
Valued Contributor

Hi,

 

How can I rotate existing views in a draft? I'm in the need to rotate the "alignment" (or what it's called), 90°.

 

See attached image.

9 REPLIES 9

Re: Draft: Rotate views

Valued Contributor
Valued Contributor

Seems I found a way to rotate a view, but only a single one and i'm not sure if that is the correct method to use...

 

Click a view, properties, set angle (see image).

Is this correct?

 

Also, I did the same to hide hidden lines, but again - only count 1 view and not all (i want hidden lines ... hidden in all views. )see image).

 

Is this correct?

 

Re: Draft: Rotate views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That looks right.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
Highlighted

Re: Draft: Rotate views

Valued Contributor
Valued Contributor

That worked, to some extend.

 

I had to remove all the other views, because it was not possible to rotate them all - they did not show correctly. I ended up rotating one, then delele all other views and use "Principal" tool to place the new views.

 

This would have been a disaster, if I had a lot of dimensions though - a lot of lost work.

 

Isnt there a better way to do this?

Re: Draft: Rotate views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't know of any way to do a mass rotate of a bunch of views. Just have to plan ahead I guess if view angle is important.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Draft: Rotate views

Valued Contributor
Valued Contributor

You can set up custom view orientations from the view wizard, drawing view layout button if the view is not already placed.  In my opinion, this would be the ideal way if you can't use a named view.  To rotate an existing view, you can do what you did in the view properties, or you can go to the Sketching tab and use the Rotate feature.  It's a pulldown within the "Move" button.

 

Matt

Re: Draft: Rotate views

Phenom
Phenom

You can set up the defaults for placing drawing views in Solid Edge Options > Edge Display (in Draft environment)

I think you will need to set them in the template file to keep the settings for all future drawings.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Draft: Rotate views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think @Kenneth was referring to already placed views possibly having annotations. Not how to initially set the views.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Draft: Rotate views

Valued Contributor
Valued Contributor

No easy solution for this it seems.

I just have to plan ahead and make sure to place the first view correctly Smiley Happy

 

The dimensions will look weird too, if you start to rotate an existing view - i guess.

Re: Draft: Rotate views

A mass rotate is impossible because those are projected views.  So if you TOTALLY change a view, then you effectivly change them all since they are projected.

 

However, another method to rotate that not even my VAR knew about during our training is to use the "Rotate" command on the sketch menu in Draft.  This will allow you to rotate the views as well.

 

But like mentioned before, planning kis key.  I too have to often redraw views if I change orientation, but because they are projected, there is absolutley no way around this.  

 

Even SolidWorks and other programs cant do it the way you are wanting.  In SW, you can change the principal view you placed first to another orinetation, but you affect any views that were projected off of that.

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments