Draft Saved as TIFF

Esteemed Contributor
Esteemed Contributor

Hi Edgers,



i have a couple of users here, which upgraded from ST7 to ST9 a few weeks ago.

What they have commented is a loss in quality when eporting drafts to tiff which is necessary (no question about is it good or is there a better method, it is a must)

 

When You compare the tiff output from a ST7 computer with a tiff from ST9 (same draft file, same rsoulution and picture size and - for me - same options and setting in SE) man can see that lines in the ST7 tiff a thicker and could be seen better - much better - than that from the ST9

 

Is there a secret setting or registry hack or an INI where man can define how thick - or better how many pixels should be used for a certain line thickness?

 

 

Thanks



regards
Wolfgang