Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft Sheet Seperation

Experimenter
Experimenter

Good Morning:

 

I am looking for a way to seperate sheets in a draft to individual drafts. Some of these have 40-75 drafts in one file. I have considered trying to come up with a plug-in ( have some VB experience), but basic information on the Solid Edge API and how to use it is almost non-existant. Is there something in Solid Edge similar to LISP in Autodesk products for automating simple tasks?

 

Any assistance in this matter would be greatly appreciated.

3 REPLIES

Betreff: Draft Sheet Seperation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dccjr3927

 

 

I think this might not be so easy as any macro recorder etc. can and will do.

 

You strictly have to use the SE API using vb.net or C.net etc.

 

Have a look at @Tushar tutorials (there just today were links to his homepage)  or have a look into the "Programers Tutorial" in the help section of SE

 

 



regards
Wolfgang

Re: Draft Sheet Seperation

Honored Contributor
Honored Contributor

If I was to so this manually, I would save the draft file 47 times and then delete the unwanted tabs in each file.

Re: Draft Sheet Seperation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

and You will do that similar using the API interface of Solid Edge I suppose.

 

Or You can copy everything what is on one sheet and paste it onto a newdraft.

The question only might be what is to set for the drafting header informations.

Which properties are to use, is the header info based upon the 3D document

related to every sheet and so on.

 



regards
Wolfgang