Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft - Variable - materialthickness to get I.D. Dimension

Experimenter
Experimenter

ID dimension.JPG

 

 

Currently I am subtracting the material thickness and typing it in the Subfix manually to show the I.D. dimension. My question is there a way to let solid edge do that calculation so I don’t have to?

Something Like (%{variable-materialthickness} I.D.)

5 REPLIES 5

Betreff: Draft - Variable - materialthickness to get I.D. Dimension

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

the only way I can imagine is to do it in 3D part itsrlve using the variable table and to expose this variable. 

 

regards
Wolfgang

Re: Draft - Variable - materialthickness to get I.D. Dimension

Honored Contributor
Honored Contributor

If you add a PMI, that can be displayed in draft.

 

I don't use that myself, but I do display plane values and even do math with the plane locations to display volumes and sizes of my sheet metal box's. I set up my models with that process in mind.

 

Any named variable (Give the PMI a name) can be displayed in draft.

If needed, set up PMI2 = PMI1+X or whatever. Then display PMI2

Re: Draft - Variable - materialthickness to get I.D. Dimension

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, you can do it, here is a video about steps:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Draft - Variable - materialthickness to get I.D. Dimension

Experimenter
Experimenter

Thanks for the video I think you’re on the right track. But, I’m not wanting to show the material thickness below the dimension I’m needing the value that is assigned to that coordinate and the suffix will take that variable and subtract the material thickness.

 

Capture.JPG

Re: Draft - Variable - materialthickness to get I.D. Dimension

Experimenter
Experimenter

This more like what Im talking about. But, I have to manually subtract the MT and my MT is 10 gauge .135Capture 2.JPG