07-07-2015 10:33 AM - edited 07-07-2015 10:43 AM
Will we ever be able to see an option to select the sheet size from the view wizard when creating a draft?
07-07-2015 10:42 AM
I made a template file for every sheet size.
Not the solution, but a workaround.
07-07-2015 10:45 AM
I have all the sheet sizes set up in the background but when bringing a model in the default size is A3 but it would be nice to select A2 or A1 from a drop down or something. It would make the drawing creation flow much quicker and easier.
07-07-2015 10:59 AM
I haven't tested it yet, but one of the reasons for me to make a single sheet template set-up in stead of on template with all the sizes is filesize.
Every draft on your server is bigger than needed because of all the extra sheets.
OK, specialy for you :
My draft for A4 is: 338 kb
With 2 A4 sheets (portrait and landscape): 361 kb
So about 23kb per sheet extra.
Indeed, not enough difference.
So, yes indeed, I would like the dropdown to.
07-07-2015 11:06 AM
we set up templates for A B C D and E sizes. Our thinking way back for not using just one file for everything. What if you delete it before backup? and many more things. But i do think it's wierd they don't have that. Way back our trainer told us to do it that way.
07-08-2015 10:13 AM
We use one sheet size for all drafts. It's CAD and most view it electronically, so no matter what sheet size you use it's all the same size when it's on a monitor and you can zoom in if needed, so we cater to that process.
07-08-2015 11:38 AM
Not sure I get the import of the question "Will we ever be able to see an option to select the sheet size from the view wizard when creating a draft?"
If sheet size up front is important to you just select it before defining views. Why add to the view wizard a selection that you would only use once per draft?
07-08-2015 11:54 AM - edited 07-08-2015 11:55 AM
Ken,
What sheet size is the one you use? Just curious.
Unfortunately, we are still stuck with actually printing drawings for manufacturing. Of course they print virtually all drawings to A size so some D size drawings are pretty tough to read, especially with my older eyes.
I try to use A for basic simple parts and B for most everything else, however our stuff is very large and can be pretty complex so I also use D a fair amount too. I try to avoid C size as a rule.
Bob Henry
07-08-2015 11:56 AM
@bshand When you use the "create drawing" from the assembly environment you are presented with the Drawing View Wizard. Our Draft template has A3 selected as the default however we may want an A2 sheet to suit the model better. So we have to place the view then click background sheet and click A2 template and click back. Having the ability to select the sheet size from a drop down would make this process a much slicker process!
When you have a lot of drawings of piece parts from an assembly to do these small things start to become irksome.
07-08-2015 12:19 PM - edited 07-08-2015 12:21 PM
I guess if I had that problem I would do some variation on what Joris suggested.
Create a draft template for each size. Whether each template has only one background sheet or if all backgrounds are there but the background size needed is default for each template. Then you select it right at the beginning of the "create drawing of active model" process.
Seems like it accomplishes the same thing.