Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft cut/paste

Gears Phenom Gears Phenom
Gears Phenom

I use copy paste fairly often on draft noting misc. things between sheets..  I'm not sure with which maint. pack or other change, but how do i get the default to be "paste to original" ?  it used to do this but now i have to select that from the pull down or press shift when placing.

-Craig
3 REPLIES 3

Re: Draft cut/paste

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could edit the ribbon to add "paste to original position"

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Draft cut/paste

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Craig_H In the Options with a Draft file open, in the General section there is a "Preferred 2D Paste Behavior" setting.  You can set your preference there.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Draft cut/paste

Gears Phenom Gears Phenom
Gears Phenom
@KennyG I knew there had to be an option!
Thanks
-Craig