Cancel
Showing results for 
Search instead for 
Did you mean: 

Draft fails to save new file

Valued Contributor
Valued Contributor

Sometimes, maybe randomly, SE ST9 fails to create a new file on the shared disk on the server: Solid Edge says that it is impossible to access to the file, and in the meanwhile a file of 0 KB is created, with the same name of the file that I was trying to save. At this point, I can save the new file to a local disk without problems.

 

After a few minutes, this "0 KB" file is deleted and it is possible to save the file to the server normally.

 

My VAR says that the issue could be related to a not stable network, but I think that the problem is due to Solid Edge: actually Solid Edge is the only sotfware in use here that shows this problem, and I'm not sure but I guess that the problem started to arise with the MP8 of ST9.

 

Workstation: Win7-x64, Server: Windows Server 2012.

 

Any experience/suggestion?

____________________________
http://www.stimarchetti.it
Design of automation
7 REPLIES

Re: Draft fails to save new file

Gears Phenom Gears Phenom
Gears Phenom

You are running built in file management, with indexing on the network drive, no? I had this issue. You need to download and install an update to the network drive.

 

Try for now, going to the network folder that you are working in and turn off indexing manually. Like right click on the folder and open properties, then uncheck indexing. See if that fixes it. If so, you need to install the update to the file management.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Draft fails to save new file

Valued Contributor
Valued Contributor

Are you referring to this update:

 

/product_updates/ST9/Maintenance_Packs/MP08/Built-in/Fast_Search_MSI_MP8.exe

 

released on 15 June 2017?

____________________________
http://www.stimarchetti.it
Design of automation

Re: Draft fails to save new file

Gears Phenom Gears Phenom
Gears Phenom

That would be the one. You can't just install on your computer though, has to be on the network machine.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Draft fails to save new file

Siemens Phenom Siemens Phenom
Siemens Phenom

Typically when this scenario occurs, some process other than Solid Edge is immediately grabbing and locking the file on disk before Solid Edge can complete the initial save of the data into the file.  Some other processes that can be grabbing and locking the file include Windows indexing, anti-virus, thumbnail display in Explorer, cloud storage solutions e.g. Drobox et. al, Distributed File System (DFS) configuration, and disk caching to name but a few.  I would look at indexing, anti-virus, and thumbnail display first as these are the most common causes I see for this type of issue.  The other listed causes are not so common but I still see them occasionally. 

 

You can use Process Explorer from Sysinternals to help determine what process is locking the file:

 

http://www.techsupportalert.com/content/how-find-out-which-windows-process-using-file.htm

Re: Draft fails to save new file

Honored Contributor
Honored Contributor

I had similar issues when starting out on a very slow network. Since we upgraded to a newer server, no issues at all. I agree with UK dave, it's a time out and file control issue.

 

Another related issues is that if you want to make a new part that has the name name as a recently deleted file from an assembly. SE needs to be compleatly shut down or ast least that assembly needs to be closed before it will let go of the old file and allow you to make a new one with the same name in it's place.

Re: Draft fails to save new file

Gears Phenom Gears Phenom
Gears Phenom

80 bucks in pretend money says that I'm right it's indexing and if the maintenence pack for the fast search is installed on the network server it fixes it.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Draft fails to save new file

Valued Contributor
Valued Contributor
Finally I decided to roll-back to MP7, and it seems that things works well, both for this error and for the built-in management that now works again.
____________________________
http://www.stimarchetti.it
Design of automation