Cancel
Showing results for 
Search instead for 
Did you mean: 

Drafting Angles for Rib protrusions

Experimenter
Experimenter

Is there a way to add a draft angle to a Rib without creating lots of draft protrusions in a model?

1 REPLY 1

Re: Drafting Angles for Rib protrusions

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Mike

In Ordered modelling there is Web Network command which should do what you want.

Note that in the video I start with a Synchronous part. I then Transition to Ordered to acccess the Web Network command. After setting the draft angle and direction I Right Click on the mouse to accept the input and action the command.

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Cheers

Mark