Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Drag Component & Detect Collision

I am trying to detect the collision of two rotating parts defined with a gear constraint but can't get it to work. This was just a test case I tried. It works for other types of constraints but not gear constraints. What I'd like to do is get the rotation to stop when a collision occurs. Any ideas?

 

(view in My Videos)

 

gear_constraint.jpg

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
7 REPLIES 7

Re: Drag Component & Detect Collision

Gears Phenom Gears Phenom
Gears Phenom

I believe that the Gear Relation is more of an animation setting than a physical relationship.

 

In this example, it looks like you could simply apply 2 separate relationships to tie the rotation(s) and set them equal in via variable table...    either floating mates, planar align, parallel, angle... 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Drag Component & Detect Collision

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon

 

 

 

what if You use the Physical Motion ?

 

This will detect real physical relations between any surfaces during the simulation

 

PS.: this is an option in Assembly - Drag Components function

 

20180118_1641.PNG

regards
Wolfgang

Re: Drag Component & Detect Collision

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Seems like it should work to me.

It highlights the faces when you use Simulate Motor with detect collisions option.

 

LMGi
www.TLMGi.com

Re: Drag Component & Detect Collision

@hawcad

 

I tried physical motion but I can't get it to work. Seems like a limitation with the gear constraint. 

 

(view in My Videos)

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10

Re: Drag Component & Detect Collision

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon

 

 

You should supress the gear relation first

Give it a try

 

regards
Wolfgang

Re: Drag Component & Detect Collision

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I also noticed that if you set the axis and then enter an angle like 1deg. then just hold down the return key

it will highlight the faces when they collide.

It will  not stop on collision for some reason though.

But this also makes me think it should work with dragging and maybe you should call it in.

LMGi
www.TLMGi.com

Re: Drag Component & Detect Collision

@JasonTitcomb

 

Very intersting observation that the collision works if the rotation is bumped in small increments. I have opened up a ticket with GTAC.

 

Thanks to everyone for their help. 

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10