Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing Compare as Standalone App

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi edgers,

with ST8 there came a great tool the drawing compare

 

Man can save the compare for further use, OK.

Question: is there a standalon app/exe to use saved comparing results without Solid Edge installed.

 

Why:

so man coul dsend the drawing compare to a customer or supplier to show what has changed

 

 

 



regards
Wolfgang
3 REPLIES

Re: Drawing Compare as Standalone App

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Wolfgang:

 

I am not at a computer that has ST 8 installed, but recall that the Compare tool has a Save button next to the Compare button which saves the comparison results to an image file.

Will this be sufficient to send across to the customer ?

 

~Tushar

Re: Drawing Compare as Standalone App

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK,

 

answering the second::

 

 

the picture would be OK so far, but as I have seen the BMP - which is actually a PNG - only shows the first image, the difference image of the draft compare.

 

I thought it might be a multiple image picture but I wasn't able to get the two others out of the "BMP"

 

I think that a common and open Draft Compare Tool without any need for a SE install would be a great thing.

 

 



regards
Wolfgang

Re: Drawing Compare as Standalone App

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

That is a nice idea @hawcad

I will ty to include this feaure in my own Drawing Compare program which I released a litle ahead of the ST 8 version.

 

~Tushar