Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing View Display Properties

Creator
Creator

Is there a way to match the Display Properties between drawing views?  When creating from the wizard, all of the views are created with the same display properties.  If I change the display properties in one view the other views retain the display properties they were created with.  You can use the principal view command to remake the views with the new display settings, but sometimes you have made a bunch of views before you realize that the display settings need to be changed and you don't want to necessarily do the same thing several times.

 

It would be nice to be able to use a match properties command or something of the like to accomplish this.

1 REPLY

Re: Drawing View Display Properties

Honored Contributor
Honored Contributor

No. One at a time as far as I know. I have the same dessire, but this is about # 250 in my list of desired of changes to the program.