Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

Solid Edge ST9 - Draft - [ aaaa.par in bbbb.dft ]

 

Why does the drawing tab name in SE show as that ^^^

It adds a random part name next to the drawing name, when the actual drawing name is bbbb.dft

it's confusing as the tab is quite small and when you have a few docs open at the same time you don't know which file the window is actually referring to.

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
12 REPLIES 12

Re: Drawing doesn't show drawing name on SE Tab

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Do you have a picture?

Re: Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

@Tushar

I've closed the file now. but when i reopen it, it sorts it self out. 

 

but just imagine what i typed previously shown where the file name is on top of a SE window

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Drawing doesn't show drawing name on SE Tab

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Glad to know the problem has gone.

May be that was only a temporary graphics glictch.

Re: Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

Hi @Tushar

The issue has come back and it has happened to an assembly now. I don't think is a graphics issue as its only the file name that's causing the confusion its not the model view. see the screen shot below: 

my assembly file is called Pack Assembly so why is it saying 'side plate.par in' before it?

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Drawing doesn't show drawing name on SE Tab

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

I think this is easy to answer.

 

You have inplace activated the part Side Plate from the assembly Pack Assembly 1340.

 

On the other hand Your image shows the assembly environment what makes this all very strange

 

Maybe You can provide a video rather than the screenshot, this could help better.

 

 

regards
Wolfgang

Re: Drawing doesn't show drawing name on SE Tab

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @MagRiz

That is because you are editing the part in context of the assembly.

 

For eg. selecting the Edit In Place command on the plate1.par in the head1.asm assembly

 

EIP01.png

 

will display this in the title bar:

 

EIP02.png

Re: Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

not sure what you mean by activated. its not activated in the sense that it is editable in the assembly. and also its not the only part that is activated in the assembly 

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

@Tushar

but i am not editing this part in the assembly. it is however opened in a sub assembly in another tab

 

Regards,

MagRiz
(ST9 User Est 01.18)

Re: Drawing doesn't show drawing name on SE Tab

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

again, we suppose that You have inplace activated it from the assembly.

And the best way to see what You are doing would be showing a video!

 

regards
Wolfgang