Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Drawing doesn't show drawing name on SE Tab

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

and BTW, opening one and the same structure/files from different start points can cause problems due to write permissions, missing when a file is in work by two or more different sessions.

 

regards
Wolfgang

Re: Drawing doesn't show drawing name on SE Tab

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Did you right-click the part in the asembly path-finder and choose one of the options: Edit 

 

EIP03.png

 

What happens if you repeatedly press Ctrl+Q in the assembly - do the other parts appear/disapper ?

 

As @hawcad has rightly said, without sharing the sequence of steps that lead to this condition, it cannot be explained. But your screen shot clearly shows the part is being edited in place using the Edit option from either the command bar or context menu.

 

Re: Drawing doesn't show drawing name on SE Tab

Valued Contributor
Valued Contributor

im definitely not editing in context. ive even closed the other files down.

 

what is Ctrl Q meant to do? i have pressed it but nothing happened

 

Regards,

MagRiz
(ST9 User Est 01.18)